International

Press

Search press releases

Lohr am Main, 2017-07-07 PI 034-17

Large Electric Drives from Rexroth are certified for marine applications

It verifiably meets all of the requirements for use in ships and offshore equipment: Resistant to vibrations, humidity and electromagnetic disturbances.

The IndraDrive ML universal inverter from Rexroth is certified by two maritime classification societies in Europe and the USA

Two marine classification societies, DNV GL and ABS, have certified the IndraDrive ML electric drive from Rexroth as “type approved” for use in ships and offshore equipment. The modular drive series covers a power range from 110 kW to up to four megawatts and supports a voltage range from 380 V to 690 V. The international certifications reduce engineering overheads for the suppliers of maritime plants.

Non-proprietary marine classification societies set the technical standards globally and test the suitability of all relevant components and assemblies for ship building and offshore applications. Now two of these societies, Det Norske Veritas Germanischer Lloyd (DNV GL) and American Bureau of Shipping (ABS), have certified the IndraDrive ML drive series from Rexroth. All of the drive components have successfully passed the comprehensive tests. The tests examined reliability at various temperatures, levels of humidity and vibrations as well as the electromagnetic compatibility and environmental aspects. With the certification, design engineers can use the drives without needing further acceptance.

IndraDrive ML can be used as a power supply and a motor inverter. This minimizes the variants, simplifies handling and reduces the storage costs for machine manufacturers and end users. The universal inverters generate a drive capacity between 110 kW and 500 kW per unit. Using a parallel connection of up to eight units, the drive capacity increases up to four MW. This means that the series covers practically all application scenarios for maritime use. It also supports the usual power supply voltages from 380 V to 690 V used in this sector.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

Search press releases


Contact

Susanne Herzlieb Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles


2021-04-12 Press Information

Bosch Bosch reveals fast and power-dense Hägglunds Atom hydraulic motor

The smallest of the Hägglunds hydraulic motors from Bosch Rexroth has been transformed. The Hägglunds Atom takes over from the existing Hägglunds CAb – supplying not only more revolutions per minute, but also far more power than motors of similar size. The result is a tiny, power-dense package ideal for mobile, marine and recycling applications.



2021-04-12 2020-07-24 Press Information Press Information

Certified Marine Repair Center opened in Istanbul and Singapore

Following the exceedingly positive experience with its own Marine Repair Centers in Central Europe (Hamburg, DE), Asia (Shanghai, CN and Busan, KR) and North America (Houston, US), Bosch Rexroth now has a local presence in the Mediterranean area (Istanbul, TR) and Southeast Asia (Singapore, SG). The repair centers are consequently oriented towards the special needs of the shipping industry. Internal supply chains and warehousing close to the port (maximum 24-hour transport route) ensure the availability of certified parts at competitive prices. Inspection and maintenance routines in accordance with classification requirements and specially trained personnel ensure compliance with the strict specifications of the classification societies.