Press

Search press releases
2021-02-23 Press Information
Bosch Rexroth defines automation trends for 2021

Bosch Rexroth expects a further boost in automation for the manufacturing industry and other segments in 2021 – driven also by the coronavirus pandemic. This is because manufacturing companies in particular are forced to further digitalize processes in order to keep production processes efficient and delivery capabilities up and running during the crisis. However, the demand for open, easy-to-use and flexible automation solutions will also increase independently of this.
2021-02-09 Press Information
The ctrlX AUTOMATION partner ecosystem is growing

With the revolutionary ctrlX AUTOMATION platform from Bosch Rexroth, users can take advantage of an open ecosystem. Thanks to the platform, they can use apps from Bosch Rexroth, applications from third-party providers or apps they have produced themselves. As a result, applications for all automation tasks are available. More and more third-party providers are joining the partner ecosystem ctrlX World. There are already three partners for HMI applications: MGA Ingenieurdienstleistungen GmbH, Mirasoft GmbH & Co. KG and Smart HMI GmbH.
2021-02-09 Press Information
Lubricated for life

The electromechanical cylinders EMC from Bosch Rexroth now have much longer lubrication intervals. Many applications even benefit from lifelong lubrication, which makes the EMC cylinders in these solutions maintenance-free. The high-precision linear motion technology with basic factory lubrication offers the manufacturers of machine tools as well as handling and automation solutions significant competitive advantages.
2021-01-26 Press Information
20,000 km without relubrication

Good news for mechanical engineers and users: the ball rail systems BSHP and ball screw assemblies BASA from Bosch Rexroth now achieve lubrication intervals which are up to four times longer. In more and more applications, they can even be used maintenance-free over the entire service life of a component. As a result, low-maintenance or maintenance-free linear motion technology minimizes operating costs and also protects the environment because less lubricant is required.
2020-12-10 Press Information
Bosch Rexroth appoints Dr. Steffen Haack as Executive Board member responsible for engineering

Effective January 1, 2021, Dr. Steffen Haack (54) will once again be a member of the Executive Board of Bosch Rexroth AG. His tasks include the engineering activities of the company and responsibility for the three business units which constitute the Industrial Hydraulics division. Haack will retain his role as Head of the Industrial Hydraulics business unit. Within the Executive Board, Dr. Marc Wucherer (51) will be in charge of the Factory Automation division.
2020-12-04 Press Information
Bosch Rexroth builds the most advanced motion system for driving simulation

With interest in driverless cars increasing all the time, and with car manufacturers looking for deeper insights into potential driving experiences, simulations have become more and more useful. Bosch Rexroth manufactured two of the most advanced motion systems in the world to be used as the basis for two modern and immersive driving simulators.
2020-11-26 Press Information
With Smart MechatroniX, Bosch Rexroth offers new solutions for the Factory of the Future

With the new Smart MechatroniX solution platform which combines best-in-class linear motion technology components with electronics and software, Bosch Rexroth is responding to market trends in factory automation on the way to the Factory of the Future. The resulting solutions can be used in a wide range of areas. Not only do they allow quick commissioning – they also offer full process transparency and ensure a short time-to-market and high productivity.
2020-11-24 Press Information
Now available for everyone: Compact control platform ctrlX CORE from Bosch Rexroth

Bosch Rexroth has defined the industrial control system of the future with its compact ctrlX CORE control system. With its open and flexible architecture, the control platform removes the boundaries between the IPC, embedded system and drive-based technology platforms. This scalable “all-purpose control system” offers numerous advantages such as a fewer component requirement and a reduced engineering effort as well as higher productivity. The embedded control system is now available in series production.
Search press releases