International

Press

Search press releases

Lohr am Main, 2021-09-22 PI 027-21

Bosch Rexroth: Open automation platform becomes an industrial ecosystem

A range of new features for ctrlX AUTOMATION and ctrlX World

  • New hardware versions, especially when it comes to CPUs and the I/O portfolio
  • New engineering services for ctrlX WORKS
  • ctrlX SERVICES portfolio expanded
  • Investment in electronics production and warehouse logistics
  • Start of the ctrlX developR Challenge: Developing innovations together

Travel the world of automation via app technology – this was Bosch Rexroth’s vision when it launched the platform ctrlX AUTOMATION in 2019. More than 300 companies are currently implementing the solution in their applications and the step from an open platform to an industrial ecosystem has now been taken with the launch of ctrlX World in 2021. Significant improvements to the solution were also made this year – and further improvements are planned.

“Industrial automation is increasingly dominated by software. We therefore need automation solutions which are geared to increasingly digitalized industry. Among other things, they should support various programming languages, offer data transmission systems and allow IT and OT to be connected in a straightforward but secure manner. Nowadays, we know that ctrlX AUTOMATION meets the automation challenges not only in mechanical engineering but also in numerous other areas such as energy, mobility and building automation”, explained Steffen Winkler, Vice President Sales of the Automation & Electrification Solutions Business Unit at Bosch Rexroth.

Since it was launched, the solution from Bosch Rexroth has evolved from an open automation platform into an industrial ecosystem. The partner network is growing all the time, adding hardware to the ctrlX AUTOMATION ecosystem and an increasing number of apps which are available for downloading from the ctrlX Store. In 2021, Bosch Rexroth also significantly expanded the range of services for the automation platform. The increasing demand for its products means that the company is now investing in its electronics production facilities, warehousing systems and logistics.

Enhanced control platform and I/O portfolio

In 2019, Bosch Rexroth presented the first version of the control platform ctrlX CORE. This version of the ctrlX CORE system can cope with approx. 70 % of all general automation applications. The control platform is now being expanded with new members and functions. Initially, these are configurable versions. They offer not only expanded interfaces but also the option to use on-board I/Os. In 2022, an extremely high-performance version will also be introduced. Through the use of the latest CPU technology, it will offer 7 to 8 times the performance of the previous ctrlX CORE. The ctrlX CORE portfolio is rounded off by an entry-level version with a reduced number of interfaces and options.

ctrlX I/O is a functionally enhanced version of ctrlX CORE and is used for a variety of purposes including horizontal and vertical integration. It offers comprehensive communication and performance enhancements as well as I/O modules geared to technologies of the future such as 5G, TSN and AI. “ctrlX I/O opens up new possibilities for users when it comes to connectivity and networking options. We are focusing particularly on co-creation. Accordingly, the ecosystem allows the integration of partner solutions. The first pilot customers with I/Os have already been validated,” explained Steffen Winkler.

New functions for engineering

With ctrlX WORKS, Bosch Rexroth makes it easy to create, provide and use functions. In addition to simplicity, the priority here is the rigorous use of web technology. With ctrlX WORKS, engineering can be carried out on ctrlX CORE via a web browser. A comprehensive portfolio of libraries and components for typical automation applications is also available.

In 2021, a wide range of new functions for even more efficient engineering processes were added. For example, ctrlX CORE can now handle docker images too. With the Software Development Kit (SDK) which is available to all developers on GitHub, users can now develop their own apps even more easily. A development environment for Python and Google Blockly which is integrated into ctrlX CORE is another highlight. As a result, users can now carry out development on the ctrlX CORE software.

When it comes to automating engineering processes, ctrlX WORKS now offers a simple, clearly structured script interface, the Automation Interface. Recurrent engineering processes can be automated via simple scripts. This reduces the work involved by 80-90 %.

Steffen Winkler said: “With the improvements made to ctrlX WORKS, we have once again reduced the engineering outlay, significantly increased the possibilities for users and raised virtual engineering to a new level.”

Services for the entire lifecycle

To ensure that users can solve their automation problems in the best way possible, Bosch Rexroth paid particular attention to accompanying services in 2021. With ctrlX SERVICES which was introduced last year and is being gradually expanded, users are offered support over the entire product lifecycle.

This year, the focus was on the ctrlX Store that was unveiled recently. Here, users can download numerous apps from Bosch Rexroth and third-party providers. The ctrlX Store offers online access to all available apps and libraries for creating applications. The ctrlX AUTOMATION ecosystem – and thus the scope of functions – can be expanded easily by downloading additional apps or integrating partner applications.

Bosch Rexroth offers the ctrlX Device Portal for launching new software functions, centrally managing and maintaining device settings or remote maintenance. The solution allows a complete service – from remote maintenance and backup/restore to the private software repository.

ctrlX developR Challenge encourages collaboration and innovation

“Many new features and improvements are the result of close collaborations with our partners and users. Our development work is thus geared to their actual needs. Innovations also come through co-creation. This prompted our ctrlX developR Challenge which is starting now,” explained Jasmin Heim, a Marketing Manager within Bosch Rexroth’s Automation & Electrification Solutions Business Unit.

The ctrlX developR Challenge is an international idea and developer competition. The aim is to apply the ideas and requirements of software developers in a practical context. Jasmin Heim is encouraging people to take part: “Ambitious software developers are invited to realize their creative ideas with the help of the ctrlX CORE control platform. The application phase will run until the end of November. After that, the solution phase during which entrants can work on new projects together with mentors will begin. During the second quarter of 2022, the winners will be announced by a renowned jury during a pitch event. It will be interesting to see what innovations result – innovations which could be used in our automation platform later on.”

Bosch Rexroth sorgt als ein weltweit führender Anbieter von Antriebs- und Steuerungstechnologien für effiziente, leistungsstarke und sichere Bewegung in Maschinen und Anlagen jeder Art und Größenordnung. Das Unternehmen bündelt weltweite Anwendungserfahrungen in den Marktsegmenten Mobile Anwendungen, Anlagenbau und Engineering sowie Fabrikautomation. Mit intelligenten Komponenten, maßgeschneiderten Systemlösungen sowie Dienstleistungen schafft Bosch Rexroth die Voraussetzungen für vollständig vernetzbare Anwendungen. Bosch Rexroth bietet seinen Kunden Hydraulik, Elektrische Antriebs- und Steuerungstechnik, Getriebetechnik sowie Linear- und Montagetechnik einschließlich Software und Schnittstellen ins Internet der Dinge. Mit einer Präsenz in mehr als 80 Ländern erwirtschafteten über 29.600 Mitarbeiter 2020 einen Umsatz von rund 5,2 Milliarden Euro.

Mehr Informationen unter www.boschrexroth.com

Die Bosch-Gruppe ist ein international führendes Technologie- und Dienstleistungsunternehmen mit weltweit rund 395 000 Mitarbeitern (Stand: 31.12.2020). Sie erwirtschaftete im Geschäftsjahr 2020 einen Umsatz von 71,5 Milliarden Euro. Die Aktivitäten gliedern sich in die vier Unternehmensbereiche Mobility Solutions, Industrial Technology, Consumer Goods sowie Energy and Building Technology. Als führender Anbieter im Internet der Dinge (IoT) bietet Bosch innovative Lösungen für Smart Home, Industrie 4.0 und Connected Mobility. Bosch verfolgt die Vision einer nachhaltigen, sicheren und begeisternden Mobilität. Mit seiner Kompetenz in Sensorik, Software und Services sowie der eigenen IoT-Cloud ist das Unternehmen in der Lage, seinen Kunden vernetzte und domänenübergreifende Lösungen aus einer Hand anzubieten. Strategisches Ziel der Bosch-Gruppe sind Lösungen und Produkte für das vernetzte Leben, die entweder über künstliche Intelligenz (KI) verfügen oder mit ihrer Hilfe entwickelt oder hergestellt werden. Mit innovativen und begeisternden Produkten sowie Dienstleistungen verbessert Bosch weltweit die Lebensqualität der Menschen. Bosch bietet „Technik fürs Leben“. Die Bosch-Gruppe umfasst die Robert Bosch GmbH sowie ihre rund 440 Tochter- und Regionalgesellschaften in rund 60 Ländern. Inklusive Handels- und Dienstleistungspartnern erstreckt sich der weltweite Fertigungs-, Entwicklungs- und Vertriebsverbund von Bosch über fast alle Länder der Welt. Mit ihren weltweit mehr als 400 Standorten ist die Bosch-Gruppe seit Frühjahr 2020 CO2-neutral. Basis für künftiges Wachstum ist die Innovationskraft des Unternehmens. Bosch beschäftigt weltweit rund 73 000 Mitarbeiter in Forschung und Entwicklung an 129 Standorten, davon etwa 34 000 Software-Entwickler.

Mehr Informationen unter www.bosch.com , www.iot.bosch.com , www.bosch-presse.de , www.twitter.com/BoschPresse .

Search press releases


Contact

Manuela Kessler Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles


2021-11-24 Press Information

Bosch Rexroth offers flexible communication architectures for the Factory of the Future

Communication – for example from machine to machine – is crucial when it comes to Industry 4.0. Bosch Rexroth and third-party providers therefore make solutions available for communicating on all levels via ctrlX World, the partner network of the ctrlX AUTOMATION system. Nokia, ifm electronic GmbH and WAGO Kontakttechnik GmbH & Co. KG. are all new ctrlX World partners.



2021-11-24 2021-11-17 Press Information Press Information

Bosch Rexroth and Schubert extend 40-year development partnership

Bosch Rexroth AG and Gerhard Schubert GmbH, which specializes in robotic packaging machines, have set out the framework for their continued future cooperation. The existing partnership, which began nearly 40 years ago, has been extended for another four years. The plan is to introduce the latest generation of cabinet-free drives based on the ctrlX AUTOMATION platform.