International

Press

Search press releases

Lohr am Main, 2021-06-30 PI 017-21

ValueStreamManager app for ActiveCockpit assists shopfloor management

The ValueStreamManager supports the continuous improvement process by digitally mapping, designing and visualizing value streams.

  • New app from Bosch Rexroth: digital mapping, design and visualization of value streams
  • Efficient planning of the material and information flow as well as high transparency
  • Potentially lower storage costs
  • Optimum sales planning and use of resources

Many production companies would like a modern lean management system in order to plan and implement the value stream in an optimum manner. But with high material stocks, bottlenecks and cycle times, it can be difficult to achieve greater productivity. This can be risky – after all, more and more customers are demanding quick delivery times and great product variance. In addition, companies are looking to use fewer materials, reduce wastage and minimize storage costs. With the introduction of the ValueStreamManagers (VSM) as part of the ActiveCockpit software, Bosch Rexroth offers a digital tool for establishing the optimum mix of flexibility and efficiency in production. With the VSM, the lean management method is used to manage continuous improvement processes and make them even more effective. Proven and new approaches are combined and expand the scope of the solution. Because it maps, designs and visualizes value streams digitally, the VSM is aimed at the entire shopfloor management.

With the ValueStreamManager, the interactive, expandable ActiveCockpit software from Bosch Rexroth takes on a new dimension, paving the way to the Factory of the Future for even for production professionals. After all, the application works not only within a production line – it works throughout the production environment. The VSM observes the entire value streams during the production process – from ordering, stock levels and assembly to deliveries to customers. In the VSM, all value-creating and non-value-creating activities are calculated and visualized transparently. The tool gathers data, visualizes the value stream and analyzes it – from the current to the target status. Up-to-date, consistent key figures provide a sound basis for making the right shopfloor management decisions quickly.

Digital support for collaboration

With the app, Bosch Rexroth not only makes shift managers’ work easier – it also assists production, value stream and lean managers in their day-to-day work. With the ActiveCockpit, the classic morning walkaround is transformed from a reactive into a proactive production tool. Thanks to paperless value streams and the multi-touch function, optimization activities become visible with just a gesture. In the ValueStreamManager, information is sent straight to the person responsible. This allows decisions to be made and acted upon more quickly. The VSM makes manual processes less susceptible to errors and, in the event of a change of plan, makes it clear what the causes are.

Greater transparency and efficiency in day-to-day operations

Unlike with conventional value stream tools and the classic paper form, bigger value streams can be split into specific, individually defined areas thanks to the VSM’s grouping function. As a result, work processes become clearer and more transparent. Particular benefits include the decoupling of value streams, the resulting reduction in complexity and the efficient planning of materials and personnel. Delayed deliveries and material wastage in production can therefore be avoided – as can bottlenecks, system breaks and excessive stock levels. As a result, storage costs can be reduced, deliveries can be made on time and sales planning and the use of resources can be optimized. The newly integrated formula calculation system makes the tool even more efficient and reliable: complex formulas no longer need to be calculated by hand – the VSM takes care of them. All employees can access these formulas, as a result of which the same formula is used throughout the plant. The VSM’s digital value stream management also reduces the adjustment period and the work involved when developing models.

Optimization thanks to mapping, design and visualization

Designed in accordance with the lean philosophy, the VSM helps to improve the production process. Optimization takes place in three steps:

  • During the digital mapping, the value stream is recorded live on the shopfloor by an employee using the app. The throughput times are automatically calculated using built-in formulas and displayed.
  • Design ensures absolute transparency: Here, possible optimization states can easily be compared, as a result of which the target state can quickly be reached.
  • In the improvement tool, Kaizen blitzes can be defined for individual cases in order to analyze faults quickly and come up with effective solutions. The KPIs are shown as bars or radar charts. The library is based on existing symbols of the process, material and information flow. The constant PDCA loop (Plan, Do, Check, Act) ensures that the changes initiated in the various areas of action can be checked at all times, generate added value and help to improve the KPIs.

Installation

The ActiveCockpit software’s user-oriented interface allows access to data regardless of location. As a result, everyone involved in the project can work in parallel while on the move. The ValueStreamManager app only needs to be installed once on the ActiveCockpit via the Admin menu. The web-based app uses browser technology for integration purposes and can be used as a complete cloud service. The VSM’s user language is German or English.

Efficient improvement with the ActiveCockpit

ActiveCockpit brings together IT applications such as production planning, the sending of e-mails and quality data management with the software functions of machines and systems. The software can be expanded quickly and easily via additional apps such as the DeviationManager or the LeanIndicator. The focus here is on the processing and visualization of production data in real time as well as the continuous improvement process: Intelligent connectivity saves time when preparing information, and all relevant information is available to everyone involved – in real time and anywhere. Clear analysis tools and measure definition round off the efficient optimization process. Companies and their customers benefit from quicker delivery times, greater efficiency and optimized standards.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries more than 29,600 associates generated sales revenue of around 5.2 billion euros in 2020.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 395,000 associates worldwide (as of December 31, 2020). The company generated sales of 71.5 billion euros in 2020. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT provider, Bosch offers innovative solutions for smart homes, Industry 4.0, and connected mobility. Bosch is pursuing a vision of mobility that is sustainable, safe, and exciting. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to facilitate connected living with products and solutions that either contain artificial intelligence (AI) or have been developed or manufactured with its help. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. With its more than 400 locations worldwide, the Bosch Group has been carbon neutral since the first quarter of 2020. The basis for the company’s future growth is its innovative strength. At 129 locations across the globe, Bosch employs some 73,000 associates in research and development, of which nearly 34,000 are software engineers.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , https://twitter.com/BoschPress

Search press releases


Contact

Manuela Kessler Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles


2021-10-06 Press Information

Ergonomic, sustainable and economical

Assembly lines often have to be adapted to new products. An ever-increasing product variance requires flexibility at the workstation. At the same time, the focus is on increasing the performance and health protection of employees. With the introduction of the SL LED Basic system lamp, Bosch Rexroth meets current and future market requirements. Thanks to the innovative DIM box, which can supply power to several lamps, the lamps are extremely compact. The new product variants not only enable flexible assembly for individual ergonomic workstations, but also offer an energy-efficient and economical solution.



2021-10-06 2021-10-05 Press Information Press Information

FRAMEpro brings Bosch Rexroth’s modular profile system into CAD environments

With the new FRAMEpro CAD plug-in, Bosch Rexroth allows its proven basic mechanic elements for machine frames and housings to be transferred straight to the CAD environments Autodesk® Inventor and SOLIDWORKS from Dassault. Users of both systems can thus reduce the engineering time and avoid errors owing to media breaks and potential incorrect entries. From now on, automatically set connections and profile configurations, automatic adjustments in the event of changes, intelligent macros and useful functions will save valuable time during planning and construction work using Bosch Rexroth’s proven modular aluminum profile system.