International

Press

Search press releases

Lohr am Main, 2021-03-23 PI 009-21

Parameterizing and reading out hydraulic valves with a smartphone and Bluetooth

New digital on-board electronics from Bosch Rexroth requires no fieldbus

With the newly developed generation of digital on-board electronics for hydraulics, Rexroth allows economical scaling between analog components and those with a fieldbus/Ethernet connection. It takes advantage of the economic benefits of digitalization with no additional cabling. The new generation provides the open interfaces Bluetooth and IO-Link. In conjunction with a suitable app, commissioning engineers, operators and service technicians can access components and change parameters using their smartphone – directly and independently of the machine control system.

The first components to feature the new digital on-board electronics are the new proportional pressure regulating valves. In terms of hardware, they offer improvements thanks to volume flow-independent pressure regulation and a linear command value-pressure characteristic curve with four pressure levels. The valves have an integrated pressure sensor as well as a connection for external pressure sensors.

During initial commissioning, the components identify themselves via their digital name plate and, after a few moments, the technicians can start the parametrization process via their smartphones. An LED lights up blue during the connection and shows the commissioning engineer which proportional pressure reduction valve they are currently connected to.

Commissioning engineers can select from Rexroth’s predefined parameter sets or define them themselves. They can then save them and transfer them to identical valves. The app’s new patented slider makes optimization even easier. When the slider is moved between “Moderate” and “Aggressive”, the app’s software automatically adjusts all corresponding parameters to the selected dynamics.

For end users, the new digital on-board electronics significantly increases flexibility for process changes. If for example a tool which is twice as heavy is used on a press, a different valve would often have to be used on previous machines. With the new generation, it is sufficient to bring up the app in order to adjust the parameters accordingly. As a result, the end user can save the money needed for a conversion and the resulting machine downtime is avoided.

In addition, end users can use condition monitoring with no additional outlay. Via the app, they call up operating data such as the temperature or operating hours using the Diagnostics button. This helps to prevent nasty surprises. Via IO-Link, users can automatically set up this status monitoring in the machine control system too. Condition monitoring extends the operating life of components and increases availability.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, roughly 31,000 associates generated sales revenue of roughly 6.2 billion euros in 2019.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 394,500 associates worldwide (as of December 31, 2020). According to preliminary figures, the company generated sales of 71.6 billion euros in 2020. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT provider, Bosch offers innovative solutions for smart homes, Industry 4.0, and connected mobility. Bosch is pursuing a vision of mobility that is sustainable, safe, and exciting. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to facilitate connected living with products and solutions that either contain artificial intelligence (AI) or have been developed or manufactured with its help. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 126 locations across the globe, Bosch employs some 73,000 associates in research and development, as well as roughly 30,000 software engineers.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , https://twitter.com/BoschPress

Search press releases


Contact

Manuela Kessler Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles


2021-10-21 Statement

Digitalization of industrial hydraulics creates added value along the entire process chain

Both the manufacturers of machines and systems and end users face increasingly stiff global competition. Investment decisions are made on a more short-term basis and OEMs need to come up with individually tailored machine and system concepts more quickly. Product variance and thus the requirements as regards the adaptability of production systems are increasing. At the same time, system availability is a key factor when it comes to productivity. In addition to all these technical issues, the mechanical and plant engineering sectors – especially hydraulics – are faced with a worsening lack of specialist staff.



2021-10-21 2021-06-29 Statement Press Information

Bosch Rexroth expands its portfolio of compact axes for industrial applications through an acquisition

By taking over an extensive technology package, Bosch Rexroth will increase its range of electrically driven, servo-hydraulic compact axes currently used primarily in industrial applications. The agreement to take over all intellectual property rights, patents and know-how of EH-D GmbH and Onovum GmbH was signed in Ulm, Germany on June 28.