International

Press

Search press releases

Lohr am Main, 2014-11-14 PI 085-14

Bosch Rexroth PC control opens the gate to new applications in production

IPC-based IndraMotion MLC from Bosch Rexroth: motion logic system and Windows operation system on one compact hardware.

IPC-based IndraMotion MLC: IT and automation on one hardware

The trend towards Connected Industry is accelerating. With the new IndraMotion MLC control version based on an industrial PC, Bosch Rexroth has merged the PLC-based motion logic system with the Windows world. Machine manufacturers can now combine IT programs and real-time motion control on one powerful hardware. Through the combination of standards for the Internet of Things, such as web-based technologies, high-level languages and Ethernet-based communication protocols, as well as Windows-based applications, the control opens up access to a variety of new applications. The software-based Open Core Engineering solution portfolio has thus been extended by an additional building block which bridges the gap between PLC and IT automation.

Until now, tasks have been clearly divided for complex applications. In order to capture analysis data, measurement data and quality data quickly, a PC is required for the process and a separate control for automation. That increases system costs, and the data exchange between both hardware control systems lengthens the cycle times. With the new form of IndraMotion MLC, Bosch Rexroth has put an end to this separation. On an industrial PC, the manufacturer can combine a motion logic system on the basis of IEC 61131-3, real-time motion functions and robotics with the Windows 7 operating system installed in parallel. The operating systems work completely independently of one another and exchange information extremely quickly. Depending on the application, the industrial PC increases the computing speed by up to 100% and can connect up to 99 servo drives via the Ethernet-based automation bus Sercos as central intelligence.

Hardware and software open to Connected Industry

The IPC control system opens up new possibilities for implementing Connected Industry approaches. The user can use both motion logic and Windows-based functions at the same time. Like all IndraMotion variants, the PC-based solution allows further access to all key functions of the control system via high-level languages, through the interface technology Open Core Interface. In doing this, manufacturers of measuring machines, for example, can use the software LabVIEW to program their processes and to control motion with over 550 Virtual Instruments (VIs) – and this without having to write a single line of PLC code.

Fast engineering

The IPC control system is fully compatible with the existing controller-based variants of IndraMotion MLC and includes a scalable system firmware for motion logic applications. For the controller variants, produced programs can be easily transferred to the new hardware. Predefined function toolkits, such as condition monitoring or technology functions, replace complicated programming with simple parameterization. The integrated engineering environment IndraWorks accelerates the whole PLC-based engineering process on the basis of open standards. Furthermore, the control system automatically takes into account all the special characteristics of fluid technology and simplifies the implementation of electro-hydraulic drives.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros. (NB: Due to a change in accounting policies, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, the Bosch Group invested some 4.5 billion euros in research and development and applied for some 5,000 patents. This is an average of 20 patents per day. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

Search press releases


Contact

Susanne Herzlieb Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles


2018-04-11 Statement

The factory of the future – how far we have come and where we are going

Imagine a factory where you could change everything apart from the floor, roof and walls within a few days or even hours? Full flexibility, individuality and scalability. This is exactly what the factory of the future is about.



2018-04-11 2016-12-05 Statement Press information

One Java to connect them all

Programmers are now also developing directly on Rexroth controls with the globally established Java technology in parallel with PLC automation. Java programming allows for quick implementation of individual applications on the IndraMotion MLC control platform, simple connection to higher-level IT systems and linking with cloud-based services. Programmers no longer have to write any PLC code for this.