International

Press

Search press releases

Lohr am Main, 2014-09-17 PI 069-14

Hydraulic Motion Control - intelligent hydraulics ready for networking

The digital axis control HMC from Rexroth

The Hydraulic Motion Control (HMC) from Rexroth: open, simple, and flexible

Automation experts all agree: in increasingly networked production environments to Industry 4.0, centralized intelligent axes are the future. Provided they can communicate via open interfaces with higher-level systems. The new Hydraulic Motion Control HMC from Rexroth meets this essential requirement. The future-proof 1-axis controller for hydraulic drives with multi-Ethernet and multi-encoder interfaces as well as PLC programming in accordance with IEC 61131-3 dovetails a wide variety of concepts.

Open communications interfaces and a migration from hydraulic functions into the software are the key prerequisites for decentralized intelligence. The new, drive-based Motion Logic System HMC from Rexroth meets these requirements with open interfaces and the best-in-class hydraulic controller.

Increasingly more machine manufacturers are using real-time Ethernet protocols for coordinated motions. Yet this is a decision they are not always free to make. Big end customers are more frequently specifying a preferred protocol in order to standardize the communication architecture. OEMs must therefore equip their series in parallel with different Ethernet variants. The HMC from Rexroth decidedly reduces the costs involved. The HMC's multi-Ethernet interface supports all standard protocols on one single piece of hardware: the automation bus Sercos, Ethernet/IP, PROFINET RT as well as EtherCAT and PROFIBUS. The HMC merges an IEC 61131-3-compliant programming language with a powerful motion control for hydraulic drives. As slave, it takes over the decentralized control of an axis where it decouples the hydraulics from the automation process.

The best-in-class hydraulic controller incorporates decades of application experience in the field of hydraulic axis control, which is depicted in ready-to-use software. The software automatically offsets the special characteristics of fluid technology. The pre-defined hydraulic functionalities encompass closed-loop position, pressure, force, and velocity control, alternating control, and open-loop controlled operation. IndraWorks software supports the commissioning, parameterization, and diagnosis of the HMC.

The HMC from Rexroth opens up new networking possibilities. With the decentralized intelligence and the multi-Ethernet interface, users can easily integrate the physical advantages of hydraulics, such as high power density and simple wear-free overload protection into modern, future-proof machine concepts.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, roughly 36,700 associates generated sales revenue of approximately 5.7 billion euros in 2013.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In 2013, its roughly 281,000 associates generated sales of 46.1 billion euros. (NB: Due to a change in accounting policies, the 2013 figures can only be compared to a limited extent with the 2012 figures). Its operations are divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. In 2013, the Bosch Group invested some 4.5 billion euros in research and development and applied for some 5,000 patents. This is an average of 20 patents per day. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com and http://twitter.com/BoschPresse

Search press releases


Contact

Susanne Herzlieb Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles


2021-10-21 Statement

Digitalization of industrial hydraulics creates added value along the entire process chain

Both the manufacturers of machines and systems and end users face increasingly stiff global competition. Investment decisions are made on a more short-term basis and OEMs need to come up with individually tailored machine and system concepts more quickly. Product variance and thus the requirements as regards the adaptability of production systems are increasing. At the same time, system availability is a key factor when it comes to productivity. In addition to all these technical issues, the mechanical and plant engineering sectors – especially hydraulics – are faced with a worsening lack of specialist staff.



2021-10-21 2021-06-29 Statement Press Information

Bosch Rexroth expands its portfolio of compact axes for industrial applications through an acquisition

By taking over an extensive technology package, Bosch Rexroth will increase its range of electrically driven, servo-hydraulic compact axes currently used primarily in industrial applications. The agreement to take over all intellectual property rights, patents and know-how of EH-D GmbH and Onovum GmbH was signed in Ulm, Germany on June 28.