International

Press

Search press releases

Lohr am Main, 2021-09-29 PI 029-21

ctrlX AUTOMATION helps to implement artificial intelligence for Kohlbacher’s fully automatic straightening center

Kohlbacher’s fully automatic HAMMERHEAD 3000 straightening center is now equipped with Bosch Rexroth’s ctrlX AUTOMATION solution. (Image source: Bosch Rexroth AG)

Company specializing in filing room equipment and saw production unlocks new potential by automating a manual reworking process

  • Artificial intelligence takes over task traditionally undertaken by saw doctors
  • Bosch Rexroth’s automation platform provides basis for AI solution
  • Greater precision and efficiency and reduced use of resources for end customers

Kohlbacher GmbH, a market leader in filing room equipment and saw production, has revolutionized an essential process for its fully automatic HAMMERHEAD 3000 straightening center: a task traditionally performed by a saw doctor is now carried out with the help of artificial intelligence. Bosch Rexroth’s ctrlX AUTOMATION platform provides the basis for the AI solution. End customers now benefit, for example, from greater precision and efficiency and reduced use of resources.

Kohlbacher GmbH’s HAMMERHEAD 3000 machine automatically tensions and straightens band saw blades which become deformed during use in sawmills. However, even new saw blades must be adapted to the particular saw. Despite the fact that the process is automated, the error rate is usually inherently around 10% - 15%. As such, manual reworking by so-called saw doctors previously needed to be carried out.

However, saw doctors are a dying breed. Siegfried Kohlbacher, Managing Director of Kohlbacher GmbH, explained: “These experts are very scarce and people are no longer entering the profession. The manual reworking of saw blades is also a very time-consuming process and costs a great deal of money. However, sawmills still require a specialist who is able to repair saw blades. An employee who has not been given specific training is unable to do this. We were therefore on the lookout for a technical solution which would carry out this task.”

Use of AI app significantly reduces straightening times

Kohlbacher therefore opted to use Bosch Rexroth's open automation platform known as ctrlX AUTOMATION. It involves the use of the components ctrlX MOTION (motion, robotics and CNC software), ctrlX DRIVE (compact drive system) and ctrlX CORE (ultra-compact control system) as well as an AI app.

Kohlbacher uses the ctrlX AUTOMATION toolkit. “The heart of the system is the ctrlX CORE control platform. The drive-integrated control system saves space in the control cabinet. Together with the drive system, it is one of the most compact solutions of its type available on the market. The open ctrlX AUTOMATION architecture gives Kohlbacher direct access to all data in the control system. This is possible thanks to the ctrlX Data Layer, the central data backbone for all process and machine data, which also makes it easier to integrate AI functions which can be written in Python for example,” explained Volker Schlotz, Head of Business Development Business Unit Automation & Electrification Solutions Bosch Rexroth.

Bosch Rexroth and Kohlbacher developed the AI solution together. The automation platform serves as the technological basis for the AI app. The AI “learns” during the process and thus minimizes leveling times and the resulting downtimes in sawmills. The AI app which can be combined with the HAMMERHEAD 3000 quickly proved successful. Siegfried Kohlbacher explained: “During the first learning phase, the straightening time could be significantly reduced. The longer the learning phases last, the better the AI can positively influence the straightening time by manipulating or putting pressure on the saw blade in a certain way.”

Innovative development for a stalling market segment

Kohlbacher has therefore managed to set new standards in a market which was at risk in the past of stalling due to a lack of innovative developments. Siegfried Kohlbacher explained: “Our AI solution is changing the market. For the first time ever, the experience of a saw doctor can be transferred to a machine and the machine can then continue learning independently. Not only can saw blades be reused but there are also no more waiting times.”

There is already increasing global demand for the machine with these features. Kohlbacher is currently checking what other machine types could be combined with ctrlX AUTOMATION and suitable apps.

“Not every machine needs artificial intelligence but the openness, connectivity and functionalities of Bosch Rexroth’s automation platform provide us, as mechanical engineers, and users with flexibility – and a huge opportunity to add value”, Siegfried Kohlbacher concluded.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries more than 29,600 associates generated sales revenue of around 5.2 billion euros in 2020.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 395,000 associates worldwide (as of December 31, 2020). The company generated sales

of 71.5 billion euros in 2020. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology.

As a leading IoT provider, Bosch offers innovative solutions for smart homes, Industry 4.0,

and connected mobility. Bosch is pursuing a vision of mobility that is sustainable, safe, and exciting. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to facilitate connected living with products and solutions that either contain artificial intelligence (AI) or have been developed or manufactured with its help. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. With its more than 400 locations worldwide, the Bosch Group has been carbon neutral since the first quarter of 2020. The basis for the company’s future growth is its innovative strength. At 129 locations across the globe, Bosch employs some 73,000 associates in research and development, of which nearly 34,000 are software engineers.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-presse.com , www.twitter.com/BoschPress .

Search press releases


Contact

Manuela Kessler Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles


2021-11-24 Press Information

Bosch Rexroth offers flexible communication architectures for the Factory of the Future

Communication – for example from machine to machine – is crucial when it comes to Industry 4.0. Bosch Rexroth and third-party providers therefore make solutions available for communicating on all levels via ctrlX World, the partner network of the ctrlX AUTOMATION system. Nokia, ifm electronic GmbH and WAGO Kontakttechnik GmbH & Co. KG. are all new ctrlX World partners.



2021-11-24 2021-11-17 Press Information Press Information

Bosch Rexroth and Schubert extend 40-year development partnership

Bosch Rexroth AG and Gerhard Schubert GmbH, which specializes in robotic packaging machines, have set out the framework for their continued future cooperation. The existing partnership, which began nearly 40 years ago, has been extended for another four years. The plan is to introduce the latest generation of cabinet-free drives based on the ctrlX AUTOMATION platform.