International

Press

Search press releases

Lohr am Main, 2016-12-05 PI 082-16

One Java to connect them all

Significantly reduced effort: Accessing Industry 4.0 cloud-based services with Java applications instead of PLC code.

Java programming integrates Rexroth controls in Industry 4.0 cloud-based services without PLC code

Programmers are now also developing directly on Rexroth controls with the globally established Java technology in parallel with PLC automation. Java programming allows for quick implementation of individual applications on the IndraMotion MLC control platform, simple connection to higher-level IT systems and linking with cloud-based services. Programmers no longer have to write any PLC code for this.

Rexroth has now embedded the Java runtime environment from Oracle – Java 8 SE Embedded – in the IndraMotion MLC motion logic system and has all of the necessary software components available. The Java applications run alone or in parallel with the PLC program and directly access over 500 control functions via the Java API of the Open Core Interface. Java technology is installed on almost all PCs and the majority of smartphones and tablets worldwide. More than nine million programmers currently work with this technology and have already created a multitude of cloud solutions and business applications. As an open standard that is supported by numerous different industries, Java guarantees higher investment security than manufacturer-specific solutions.

Download programs for flexible production

Machine manufacturers, software companies and end users can now develop their own Java-based applications, service concepts and business models with little effort, or buy programs inexpensively for Rexroth control. Rexroth uses an OSGi framework as the basis for Java development. With this, several Java applications run in parallel and can be exchanged during operation. In this way, within a flexible production system, users can install changing Java programs onto the control to adapt production for new requirements – smaller batch sizes without changeover times – or to gain additional process and service information.

Cloud applications ready for use in a few days

All relevant suppliers of cloud-based services offer largely completed Java solutions for registration, login and the secure exchange of data. These functions now have direct access to the Rexroth controls. This means that complex custom client programming on the PLC level is not necessary. Companies can concentrate on identifying, collecting and transferring the relevant parameters for evaluation in the cloud. An experienced Java programmer only needs a few days to create such a solution. They do not need to write any new PLC programs for it.

Higher availability through data evaluation

The combination of Java apps, PLC program and cloud services allows the continuous monitoring of the process quality and all operating conditions. A local Java app that is connected with a cloud service can therefore send status data of the PLC program independently of the operating condition. This strengthens the informative value of condition monitoring and the predictive maintenance concepts based on this. The first applications of these smart services from Rexroth show significantly increased availability.

WebConnector universal translator

With the WebConnector "universal translator", Rexroth offers a first custom Java application for the IndraMotion MLC control system. It allows web applications based on HTML5 and Javascript direct access to control functions with different end devices such as smartphones or tablets without increased programming effort. This further simplifies the development of web-based diagnosis, visualization or analysis apps.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

Search press releases


Contact

Susanne Herzlieb Maria-Theresien-Straße 23 97816 Lohr am Main Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles


2018-04-11 Statement

The factory of the future – how far we have come and where we are going

Imagine a factory where you could change everything apart from the floor, roof and walls within a few days or even hours? Full flexibility, individuality and scalability. This is exactly what the factory of the future is about.



2018-04-11 2016-08-11 Statement Press Information

The five most expensive savings ideas for the maintenance of machinery and equipment

Machine downtime is always expensive, especially if a whole production line comes to a standstill as a result. For new machinery, the machine manufacturer is still liable, but afterwards the responsibility for maintenance lies solely with the user. Maintenance staff must constantly justify their "unproductive" costs and, hence, try to reduce them. However, some short-term saving ideas lead to nothing but higher total costs in the end. The following are the five most expensive, and unfortunately, not uncommon errors when it comes to machine maintenance.